1 - conditions of use and back-up copy
MGE UPS SYSTEMS confers to the user the non-exclusive and non-transferable
right to use the software and the documentation.
The user is permitted to make back-up copies and to reproduce the software
and the associated documentation.
2 - licence period
This licence agreement runs for 20 years from the date of acceptance.
It can be terminated
by MGE UPS SYSTEMS without warning if any part of agreement is violated.
3 - limited warranty
The warranty
is limited to the replacement of the software due to defects in the
storage medium (defects in manufacturing or materials) which are reported
within 90 days of the date of receipt.
All risks resulting
from the performance of the software are assumed by the user.
MGE UPS SYSTEMS cannot be held responsible in any way for direct or
indirect damage resulting from the use or inability to use the software,
even if MGE UPS SYSTEMS was forwarned of the risks incurred.
4 - miscellaneous
All litigation resulting from this licence agreement will be submitted
to the commercial court of Grenoble which is granted exclusive rights
of judgement.